Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
The setting form of this command performs two functions for the current system type: (1) sets the additive white gaussian noise (AWGN) level (see CALL:AWGNoise[:INTernal]:POWer:AMPlitude[:SELected]) and (2) turns the AWGN on/off state (see CALL:AWGNoise[:INTernal]:POWer:STATe[:SELected]) to on. |
|
Setting |
Range:+35dBm/1.28MHz to -165dBm/1.28MHz Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
-60.0 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:AWGNoise:POWer -60" |
|
Function |
The setting form of this command performs two functions for the TD-SCDMA system type: (1) sets the additive white gaussian noise (AWGN) level (see CALL:AWGNoise[:INTernal]:POWer:AMPlitude:TDSCdma) and (2) turns the AWGN on/off state (see CALL:AWGNoise[:INTernal]:POWer:STATe:TDSCdma) to on. |
|
Setting |
Range:+35dBm/1.28MHz to -165dBm/1.28MHz Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
-60.0 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:AWGNoise:POWer:TDSCdma -80" |
|
Function |
Sets/queries the additive white gaussian noise (AWGN) level when the AWGN power state is on for the current system type. The optional [:SELected] keyword in this command specifies that the cell power level being set or queried applies to the current system type. |
|
Setting |
Range:+35dBm/1.28MHz to -165dBm/1.28MHz Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
-60.0 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:AWGNoise:POWer:AMPLITUDE -80" |
|
Function |
Sets/queries the additive white gaussian noise (AWGN) level when the AWGN power state is on for the TD-SCDMA system type. |
|
Setting |
Range:+35dBm/1.28MHz to -165dBm/1.28MHz Resolution:0.01 |
|
Query |
same as setting |
|
*RST Setting |
-60.0 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:AWGNoise:POWer:AMPLITUDE:TDSCdma -80" |
|
Function |
Sets/queries the additive white gaussian noise power state for the current system type. The optional [:SELected] keyword in this command specifies that the cell power level being set or queried applies to the current system type. |
|
Setting |
Range:1|ON|0|OFF |
|
Query |
Range:1|0 |
|
*RST Setting |
OFF |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:AWGNoise:POWer:STATe OFF" |
|
Function |
Sets/queries the additive white gaussian noise power state for the TD-SCDMA system type. |
|
Setting |
Range:1|ON|0|OFF |
|
Query |
Range:1|0 |
|
*RST Setting |
OFF |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:AWGNoise:POWer:STATe:TDSCDMA OFF" |