Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the operating mode of the base station emulator. |
|
Setting |
Range: CALL (Active Cell ) | TDTest (TD-SCDMA Test Mode) | CW | OFF (Cell Off) |
|
Query |
CALL | CW | TDT | OFF |
|
*RST Setting |
CALL |
|
Requirements |
Test Application Revision: A.01.00 and above Test Application Revision: A.02.00 added CALL and OFF. |
|
Programming Example |
"CALL:CELL:OPERating:MODE OFF" |