SYSTem:AUDio

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions

SYSTem:AUDio:OUTPut:SOURce

Function

Set/queries whether the audio generator signal or the FM demodulation signal is selected to be routed to the AUDIO OUT port of the test set's front panel.

Setting

Range: AFGenerator|FMDemod

Query

Range: AFG|FMD

*RST Setting

AFG

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SYSTem:AUDio:OUTPut:SOURce FMDemod"

SYSTem:AUDio:OUTPut:FMDemod:BPFilter:STATe

Function

Sets/queries whether the fixed bandpass filter is inserted or bypassed in the FM Demod signal path. It is useful only when FM Demod signal is selected for output at the front-panel AUDIO OUT port.

When the state is ON, a 300 Hz to 3 KHz bandpass filter is inserted in the audio signal path. When the state is OFF, the bandpass filter is bypassed in the audio signal path.

Setting

Range: 0|OFF|1|ON

Query

Range: 0|1

*RST Setting

0 (OFF)

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SYSTem:AUDio:OUTPut:FMDemod:BPFilter:STATe ON"

SYSTem:AUDio:OUTPut:FMDemod:EXPandor:STATe

Function

Sets/queries whether the expandor filter is inserted or bypassed in the FM Demod signal path. It is useful only when FM Demod signal is selected for output at the front-panel AUDIO OUT port.

When the state is ON, the expandor filter is inserted in the audio signal path. When the state is OFF, the expandor filter is bypassed in the audio signal path.

Setting

Range: 0|OFF|1|ON

Query

Range: 0|1

*RST Setting

0 (OFF)

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SYSTem:AUDio:OUTPut:FMDemod:EXPandor:STATe ON"

SYSTem:AUDio:OUTPut:FMDemod:DEEMphasis:STATe

Function

Sets/queries whether the deemphasis filter is inserted or bypassed in the FM Demod signal path. It is useful only when FM Demod signal is selected for output at the front-panel AUDIO OUT port .

When the state is ON, the deemphasis filter is inserted in the audio signal path. When the state is OFF, the deemphasis filter is bypassed in the audio signal path.

Setting

Range: 0|OFF|1|ON

Query

Range: 0|1

*RST Setting

0 (OFF)

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SYSTem:AUDio:OUTPut:FMDemod:DEEMphasis:STATe ON"