SYSTem:BEEPer

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions

SYSTem:BEEPer:STATe

Function

Sets/queries the beeper state of the test set.

Setting

Range: 0|OFF | 1|ON

Query

Range: 0|1

*RST Setting

1 (on)

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SYSTem:BEEPer:STATe OFF"