Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
Function |
Sets/queries the state of the Restart on Fatal Error parameter. |
Setting |
Range: ON|1|OFF|0 |
Query |
Range: 1|0 |
*RST Setting |
0 |
Requirements |
Test Application Revision: A.01.00 and above |
Programming Example |
"SYSTem:FATal:ERRor:RESTart ON" |