Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Performs a full preset of the test set. This is the remote equivalent of pressing the SHIFT Preset keys on the front panel of the test set. All parameters are set to their default values. All measurements are aborted the trigger arm is set to continuous. The *RST command will set the trigger arm to single. |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTEM:PRESET2" |
|
Function |
Performs a partial preset. This is the recommended command for users when a partial preset is needed during remote operation of the test set. Any call in process is disconnected and all measurements are aborted and inactivated. Measurement parameters are not changed. A partial preset will not modify any measurement settings including trigger arm. |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTEM:PRESET3" |