Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
Function |
Sets/queries the local time of day. UTC time will track changes made directly to local time settings. Also, if new settings are made to UTC time, local time will track UCT time. Changes to time zone will cause changes to local time, but will not directly affect UTC time. |
Setting |
Range:
|
Query |
Range: "<hour>,<minute>,<second>" |
*RST Setting |
This feature is not affected by instrument preset |
Requirements |
Test Application Revision: A.01.00 and above |
Programming Example |
"SYSTem:TIME 11,10,10" |