Last updated: January 16, 2009
This section is only applicable to the lab application or a test application with the required feature license.
12.2k RMC + HSDPA
or 12.2k RMC + HSPA.
Measurement Timeout
to
On
, ensure that the
Measurement Timeout
value is greater than the time the measurement needs to measure the desired
Number of blocks to test
.
Trigger Arm
is set to
Single
, you must press the
START SINGLE
key to initiate the measurement.
Trigger Arm
to
Single
.
FDD Test
operating mode, the test set does not signal the
CQI Feedback Cycle (k)
or
CQI Repetition Factor
to the UE, you must set the values manually in the UE. To ensure a valid
Median CQI
result, you must ensure that
CQI Feedback Cycle (k)
is greater than or equal to
CQI Repetition Factor
* 2ms (so that there are no collisions between new and repeated CQI information). See
CQI Transmission Settings
for more information about this requirement.Check to see if an integrity indicator other than 0 (normal) was returned with the measurement result (see Integrity Indicator ).
Questionable MS-to-Cell Data
(28) is returned, the setting you've chosen for
Ack-Nack Repetition Factor
is causing collisions between data being sent to the UE by the test set, and the repeated ACKs/NACKs being sent by the UE. You must ensure that the minimum inter-TTI of the active HSDPA channel is greater than or equal to
Ack-Nack Repetition Factor
* 2 ms (so that there are sufficient unused subframes on the uplink for the ACK/NACK repeats to be transmitted without colliding with new ACK/NACK information). Otherwise, the repeated ACK/NACK information will be sent by the UE when the test set expects ACK/NACK information for the block it just transmitted to the UE (a block that the UE ignored because it was sending an ACK or NACK repeat for a prior block). The test set would then treat the ACK/NACK repeat like ACK/NACK information for the current block, resulting in incorrect HSDPA BLER results.
Measurement Timeout
(2) is returned, the value you entered for the measurement may be too small for the
Number of blocks to test
. In this case, either reduce the number of blocks to test or increase the timeout value.
Unsupported Configuration
(22) is returned, you must set
Channel Type
to
12.2k RMC + HSDPA
.