N1010200A Manufacturing Package

Package License:
L-MFG
Flex Apps:
FlexDCA

The N1010200A Manufacturing Package License (L-MFG) includes features optimized for using the DCA-X in a manufacturing environment.

This package enables the Manufacturing Package features which are identified in the yellow column (L-MFG) of the following table. If an L-MFG feature is also offered in another package, a bullet is also shown for that package. However, the L-RND and L-SNT columns only show shared features.

When installed, the remote *OPT? query returns a comma-delimited string that includes the L-MFG field.

FlexDCA Features in Manufacturing License Package

For FlexDCA, this table shows all the available features for the L-MFG license package (highlighted yellow background). If a feature is also available in another package license, this is marked in non-highlighted columns. The table includes active links to feature topics that are available in this help.

OPT?1 Feature FlexDCA Package Licenses FlexOTO Package Licenses
N1010100A
(L-RND1)
N1010200A
(L-MFG1)
N1010300A
(L-SNT1)
N1002000A
(L-OTO1)
N1002014A
(L-OTO171)
N1002048A
(L-OTO481)
N1002128A
(L-OTO1281)
F-AEYE Advanced Eye Analysis ■
F-AFR Automatic Fixture Removal in TDR Mode ■
F-AOP AWG Waveform Optimization ■
F-ATDR Enhanced Impedance and S-Parameters ■ ■
F-AWG Keysight Arbitrary Waveform Generator Control ■
F-C03 Output Jitter Measurements on Composite Histogram of R03/F30 Edges. ■
F-CSIG Chord Operators (CNRZ-5-EE, ENRZ) ■
F-CTDQ Codeword Error Ratio Transmitter and Dispersion Eye Closure Quaternary measurement for PAM4 ■ ■
F-DCLK Direct Clock ■
F-DFE DFE Enhancements: Pulse Response Optimization. ■
F-ENH1 Enhancements 2020 ■ ■ ■
F-EECQ Electrical Eye Closure Quaternary measurement ■

■

F-EQ Equalizers (CTLE, DFE, LFE) ■
F-ESP Extended S-Parameters ■
F-FDR Fractional Divide Ratio ■ ■
F-FEYE FlexEye Independent Eye Acquisition and Analysis ■ ■
F-FLEX FlexDCA Remote Access Software ■ ■ ■
F-FTUNE Fast Acquisition for DUT Tuning ■ ■ ■ ■
F-INF Remote connection from FlexRT on a PC to a UXR-series oscilloscope. ■
F-INR Intrinsic Noise Reduction when using a Precision Time Base. ■

■

F-IREP Instrument Report. ■ ■ ■
F-JIT Enhanced Jitter Analysis ■
F-JSA Jitter Spectrum Analysis and SW Clock Recovery Emulation ■ ■
F-LEV PAM Inner Level Amplitude Adjustment ■
F-LSNR Low SNR TDECQ ■ ■ ■ ■ ■
F-MMFE Multi-Mode Fiber Emulation for TDECQ Measurements ■ ■
F-OTO FlexOTO (Optical Test Optimizer) ■ ■ ■ ■ ■
F-PAM PAM-N Analysis Software ■ ■
F-PAT Pattern Waveform Analysis ■
F-PCOM Compensates pattern distortion in the recovered clock ■ ■ ■ ■ ■ ■
F-PEAK Peak Measurements at Hit Ratio: Overshoot, Undershoot and Peak to Peak Amplitude. ■ ■
F-PEECQ Partial Electrical Eye Closure Quaternary measurement ■
F-PFIT Adds a Pulse Fit signal processing operator. ■
F-PLL FlexPLL application that measures Jitter Transfer Function on devices with a PLL. ■
F-PMASK PAM4 Mask Test Measurements. ■ ■
F-POJ Phase-Only Timing Jitter measurements ■
F-PTDQ Partial TDECQ, Noise Margin, and SER Measurements ■
F-RAN Random Noise: Bandwidth limiting and 802.3cd (η0) support ■
F-RRX Provides a reference receiver Waveform Signal Processing operator that allows joint FFE/DFE optimization ■ ■
F-SIM InfiniiSim-DCA Waveform Transformation Toolset ■
F-SKP Specify pattern for equalizers and jitter mode ■
F-SNDR Signal-to-Noise-and-Distortions Ratio (SNDR) Feature ■
F-SW17 FlexOTO 17 Port Switch Support ■
F-SW48 FlexOTO 48 Port Switch Support ■
F-SW128 FlexOTO 128 Port Switch Support ■
F-SWITCH Optical Switch Direct Control ■ ■ ■ ■ ■
F-TDEC NRZ TDEC Measurement ■ ■
F-TDQ TDECQ Measurement and Equalizer ■ ■
F-UDI Unrestricted Data File Import ■ ■ ■ ■ ■
F-UDMO User Defined Measurements and Operators ■ ■
F-VEC VEC Measurements. ■ ■

Characters that identify a feature in the string returned by the *OPT? common programming query.