N1002000A. FlexOTO Basic Optimization
The N1002000A FlexOTO Basic Optimization Package License (L-OTO) enables the FlexOTO application without an optical switch (F-OTO feature).
When installed, the remote *OPT? query returns a comma-delimited string that includes the L-OTO field.
FlexDCA Features in a Without Switch Control License Package
For FlexDCA, this table shows all the available features for the L-OTO license package (highlighted yellow background). If a feature is also available in another package license, this is marked in non-highlighted columns. The table includes active links to feature topics that are available in this help.
Characters that identify a feature in the string returned by the *OPT? common programming query.