About FlexPLL
Click Help > About FlexPLL to view information about your version of FlexPLL. You can use this information when you need to contact Keysight Technologies technical support.
The application name, model number, and computer serial number are listed at the top of the dialog. The model numbers for the various Flex applications are listed in the following table. You can also return this information remotely using the SCPI common command *IDN? query. Installed options can be returned using the SCPI *OPT? query.
| Application | Model Number |
|---|---|
| FlexDCA (on N1000A) | N1000A |
| FlexDCA (on PC) | N1010A |
| FlexPLL | N1000100A |
| FlexOTO (Hardware Diagram) | N1000300A |
| FlexOTO (Station) | N1000200A |
System Information
Software options are listed along with the application name. The dialog also provides the URL for locating the FlexPLL web page for Keysight.com. You can always download the latest firmware from the following site:
- www.keysight.com/find/flexdca_download
Click Copy to Clipboard to place the information shown on the dialog as a list of ASCII text in Windows clipboard.
Click Save Support Info to save the file FlexDcaSupport.zip on the Windows desktop. This file is useful in the unlikely event that you experience a problem with FlexPLL for which you need to contact Keysight support. This file contains important diagnostic information that may help Keysight support to resolve the issue. A remote SCPI command is not provided for saving support information.
To save a report on current measurements and system information (PC or N1000A), save an Instrument Report file.
Click More... for the following information on third party licenses as well as open source terms and conditions.
Third-party licenses and open-source terms and conditions can be found in the Phase-Locked Loop Analysis installation directory. To the extent you are entitled to a copy of the source code for open-source software distributed with this product, a free copy will be provided. Please contact us at https://www.keysight.com/find/contactus with your request.
End-User License Agreement (EULA)