Response Memories

Use the Response Memories dialog to load saved Responses into the selected Memory, view the Response memory on the Jitter Transfer Function graph, and to customize the display of the memory's plots. Four Response memories are available.

Response files include calibration data, so there is no need to load a corresponding calibration file.

Dialog Contents

Click to turn the display of the loaded Memory plots on or off.

Click to give the loaded Memory plots a custom name or reset the name to its default value.

Click to change the color of the Memory plots. After selecting the color, close the Color dialog.

Click these buttons to load a saved Response file (*.rspx) into the selected Response memory, reload a file already in memory, or clear file data from the memory. By default, Response files are saved in the \Responses user data folder.

Responses Folder in User Folders

Click to load the currently displayed Response into the selected Response memory.

Select to display response flatness measurements.

 

Display Flatness Measurement's Effect on Measurements Displayed
Measurement Display Flatness Measurements
Setting
Maximum ■
Minimum ■
Average ■
Bandwidth ■ ■
Peaking ■ ■
Gain Frequency 1 ■ ■
Zero Frequency 1 ■ ■
Pole Frequency 1 ■ ■
Footnotes:
1. Displayed if Model Measurements selected in PLL Model Settings dialog.

Click to open the PLL Model Settings dialog from which you can display model plots and configure the model.