:EMEMory:SIGNal:TYPE

Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4

Command Syntax

:EMEMory{1:8}:SIGNal:TYPE {UNSPecified | NRZ | PAM4}

Where the required specifier {1:8} identifies one of eight eye memories.

Query Syntax

:EMEMory{1:8}:SIGNal:TYPE?

Description

Specifiies the signal type that is stored in color-grade gray-scale memory. The default value is unspecified (UNSPecified).

The PAM4 argument is only available if options 9FP or 9TP PAM-N Analysis software license is installed.

Requires FlexDCA revision A.04.50 and above.

Example Command

:EMEMory3:SIGNal:TYPE PAM4