Step 3 - Installing the IVI Compliance Package

Installation Steps: 1 2 3 4 5 6 7 8 9

Perform this step only if you are using the N603xA/M933xA or N824xA arbitrary waveform generator. Otherwise, proceed to next step.

Visit www.ni.com to download and install IVI Compliance Package 4.1 (includes the IVI Shared Components).

Only use IVI Compliance Package 4.1. The IVI Shared Components included in other versions may not be compatible with the arbitrary waveform generator drivers installed in step 5.