Understanding The Interactive IO Display
This section introduces you to the Interactive IO Graphical User Interface (GUI). You will learn how to navigate through the GUI elements and view some features and functions before you begin working with the interface.
The InteractiveIO Display
[IO Interactive: Linux]
| # | Description |
|---|---|
| 1 |
The Connection Details section displays the connection information for the connected instrument.
|
| 2 |
: Opens the Interactive IO Help and provides technical support contact information. |
| 3 |
: Toggles between dark and light themes. |
| 4 | The Connection Status bar displays the state of the connection with the instrument, along with the resource string used for establishing the connection. |
| 5 |
The Action bar includes buttons to perform various actions on the instrument:
|
| 6 |
The Command panel let's you send commands and receive response from the connection instrument.
|
| 7 | The Instrument Session History pane shows a listing of recent activity (including errors if any). |
| 8 | The Copy button appears on the selected row or beneath the mouse pointer when hovering. It allows you to copy the content of the row to the clipboard. |
| 9 | Service Status: Connected indicates that the Interactive IO service is available. If the service is interrupted and the status shows Disconnected, you must restart the Interactive IO service.
|
| 10 | IOLS version: shows the IOLS version installed on the test station. |
: Opens the Interactive IO Help and provides technical support contact information.
: Toggles between dark and light themes.