IBaseMessage::Clear
Description
Performs an IEEE 488.1-style clear of the device. VXI uses the Word Serial Clear command, and GPIB uses the Selective Device Clear command.
VB Prototype
Clear(
                                        
)
	
C++ Prototype
HRESULT Clear(
                                        
);
	
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, IOProtocol, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Clear, ReadSTB, IBaseMessage Overview