IBaseMessage::SpecVersion
Description
The VISA-defined version information for the specification version to which this component complies.
VB Prototype
Dim value As Long
                                            value = object.SpecVersion
                                        
C++ Prototype
HRESULT get_SpecVersion(
                                        
  long* SpecVersion
);
		
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, IOProtocol, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Clear, ReadSTB, IBaseMessage Overview