IEventGpibCIC::Close
Description
Closes the resource. Sending the resource's COM object's reference count to zero (and thus destroying the object) also executes a close, but this method may be useful for environments with garbage collection or other facilities that make object lifetimes non-deterministic.
VB Prototype
Close(
                                        
)
	
C++ Prototype
HRESULT Close(
                                        
);
	
Return Value
Refer to the table of return codes.
See Also
type, CustomEventTypeNumber, CICState, GetAttribute, SetAttribute, Close, IEventGpibCIC Overview