IEventGpibCIC::GetAttribute
Description
Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces.
VB Prototype
value As 
				Variant = GetAttribute(
                                        
  attribute As Long
)
	
C++ Prototype
HRESULT GetAttribute(
                                        
  long attribute,
  VARIANT* pAttrState
);
	
Parameters
attribute
The attribute type to retrieve.
pAttrState
The value of the attribute.
Return Value
Refer to the table of return codes.
See Also
type, CustomEventTypeNumber, CICState, GetAttribute, SetAttribute, Close, IEventGpibCIC Overview