IEventManager::HardwareInterfaceName

Description

The name of the hardware interface (GPIB, ASRL, etc.).

VB Prototype

Dim value As String
value = object.HardwareInterfaceName

C++ Prototype

HRESULT get_HardwareInterfaceName(
  BSTR* HardwareInterfaceName
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, MaximumQueueLength, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, EnableEvent, DisableEvent, DiscardEvents, WaitOnEvent, InstallHandler, UninstallHandler, IEventManager Overview