IEventManager::ResourceName

Description

The VISA resource name of the currently open resource. This name is the canonical version of the resource name and therefore may vary from the resource string used to open/init the resource.

VB Prototype

Dim value As String
value = object.ResourceName

C++ Prototype

HRESULT get_ResourceName(
  BSTR* ResourceName
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, MaximumQueueLength, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, EnableEvent, DisableEvent, DiscardEvents, WaitOnEvent, InstallHandler, UninstallHandler, IEventManager Overview