IEventVxiSignal::Close
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Closes the resource. Sending the resource's COM object's reference count to zero (and thus destroying the object) also executes a close, but this method may be useful for environments with garbage collection or other facilities that make object lifetimes non-deterministic.
VB Prototype
Close(
                                        
)
	
C++ Prototype
HRESULT Close(
                                        
);
	
Return Value
Refer to the table of return codes.
See Also
type, CustomEventTypeNumber, SignalStatusID, GetAttribute, SetAttribute, Close, IEventVxiSignal Overview