IEventVxiSignal::SignalStatusID
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
The 16-bit Status/ID value retrieved during the IACK cycle or from the Signal register.
VB Prototype
Dim value As Short
                                            value = object.SignalStatusID
                                        
C++ Prototype
HRESULT get_SignalStatusID(
                                        
  short* SignalStatusID
);
		
Return Value
Refer to the table of return codes.
See Also
type, CustomEventTypeNumber, SignalStatusID, GetAttribute, SetAttribute, Close, IEventVxiSignal Overview