IMessage::HardwareInterfaceNumber

Description

The board number of the hardware interface.

VB Prototype

Dim value As Short
value = object.HardwareInterfaceNumber

C++ Prototype

HRESULT get_HardwareInterfaceNumber(
  short* HardwareInterfaceNumber
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, IOProtocol, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Clear, ReadSTB, Read, ReadString, Write, WriteString, IMessage Overview