IMessage::IOProtocol
Description
The protocol type for I/O communication with the physical resource.
VB Prototype
Dim value As IOProtocol
value = object.IOProtocol
object.IOProtocol = value
C++ Prototype
HRESULT get_IOProtocol(
IOProtocol* IOProtocol
);
HRESULT put_IOProtocol(
IOProtocol IOProtocol
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, IOProtocol, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Clear, ReadSTB, Read, ReadString, Write, WriteString, IMessage Overview