IPxi2::AllowWriteCombine

Description

Get or Set the PXI Allow Write Combine.

VB Prototype

Dim value As Boolean
value = object.AllowWriteCombine

object.AllowWriteCombine= value

C++ Prototype

HRESULT get_AllowWriteCombine(
  VARIANT_BOOL* AllowWriteCombine
);

HRESULT put_AllowWriteCombine(
  VARIANT_BOOL AllowWriteCombine
);

Return Value

Refer to the table of return codes.

See Also

ActualLinkWidth, AllowWriteCombine, BusNumber, ChassisNumber, Close, ComponentVersion, DevNumber, DstarBusNumber, DstarLineSet, FuncNumber, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, Init, IsExpress, LastStatus, LockRsrc, LockState, MaxLinkWidth, MemBaseBar0, MemBaseBar1, MemBaseBar2, MemBaseBar3, MemBaseBar4, MemBaseBar5, MemSizeBar0, MemSizeBar1, MemSizeBar2, MemSizeBar3, MemSizeBar4, MemSizeBar5, MemTypeBar0, MemTypeBar1, MemTypeBar2, MemTypeBar3, MemTypeBar4, MemTypeBar5, OptionString, ProgID, ResourceName, SessionType, SlotLinkWidth, SlotLocalBusLeft, SlotLocalBusRight, SlotOffset, SlotPath, SlotWidth, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, SpecVersion, StarTriggerBus, StarTriggerLine, Timeout, TriggerBus, UnlockRsrc, IPxi2 Overview