IPxi2::SlotPath
Description
Returns the slot path.
VB Prototype
Dim value As String
value = object.SlotPath
C++ Prototype
HRESULT get_SlotPath(
BSTR* SlotPath
);
Return Value
Refer to the table of return codes.
See Also
ActualLinkWidth, AllowWriteCombine, BusNumber, ChassisNumber, Close, ComponentVersion, DevNumber, DstarBusNumber, DstarLineSet, FuncNumber, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, Init, IsExpress, LastStatus, LockRsrc, LockState, MaxLinkWidth, MemBaseBar0, MemBaseBar1, MemBaseBar2, MemBaseBar3, MemBaseBar4, MemBaseBar5, MemSizeBar0, MemSizeBar1, MemSizeBar2, MemSizeBar3, MemSizeBar4, MemSizeBar5, MemTypeBar0, MemTypeBar1, MemTypeBar2, MemTypeBar3, MemTypeBar4, MemTypeBar5, OptionString, ProgID, ResourceName, SessionType, SlotLinkWidth, SlotLocalBusLeft, SlotLocalBusRight, SlotOffset, SlotPath, SlotWidth, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, SpecVersion, StarTriggerBus, StarTriggerLine, Timeout, TriggerBus, UnlockRsrc, IPxi2 Overview