IVxi3::DestinationAccessPrivilege
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Specifies the address modifier to be used in high-level access operations, such as OutXX and MoveOutXX, when writing to the destination.
VB Prototype
Dim value As VXIMemoryAccessPrivilege
                                            value = object.DestinationAccessPrivilege
                                        
object.DestinationAccessPrivilege = value 
                                        
C++ Prototype
HRESULT get_DestinationAccessPrivilege(
                                        
  VXIMemoryAccessPrivilege* DestinationAccessPrivilege
);
		
HRESULT put_DestinationAccessPrivilege(
                                        
  VXIMemoryAccessPrivilege DestinationAccessPrivilege
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, CommanderLA, DestinationAccessPrivilege, DeviceClass, FastDataChannel, FastDataChannelMode, FastDataChannelUsePair, ImmediateServant, LogicalAddress, MainframeLogicalAddress, ManufacturerID, ManufacturerName, MemoryBase, MemorySize, MemorySpace, ModelCode, ModelName, TriggerID, Slot, SourceAccessPrivilege, TriggerSupport, Is4882Compliant, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, CommandQuery, IVxi3 Overview