IVxi3::SourceAccessPrivilege
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Specifies the address modifier to be used in high-level access operations, such as InXX and MoveInXX, when reading from the source.
VB Prototype
Dim value As VXIMemoryAccessPrivilege
                                            value = object.SourceAccessPrivilege
                                        
object.SourceAccessPrivilege = value 
                                        
C++ Prototype
HRESULT get_SourceAccessPrivilege(
                                        
  VXIMemoryAccessPrivilege* SourceAccessPrivilege
);
		
HRESULT put_SourceAccessPrivilege(
                                        
  VXIMemoryAccessPrivilege SourceAccessPrivilege
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, CommanderLA, DestinationAccessPrivilege, DeviceClass, FastDataChannel, FastDataChannelMode, FastDataChannelUsePair, ImmediateServant, LogicalAddress, MainframeLogicalAddress, ManufacturerID, ManufacturerName, MemoryBase, MemorySize, MemorySpace, ModelCode, ModelName, TriggerID, Slot, SourceAccessPrivilege, TriggerSupport, Is4882Compliant, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, CommandQuery, IVxi3 Overview