Keysight VISA.NET Help
IMessageBasedSession Interface Methods

For a list of all members of this type, see IMessageBasedSession members.

Public Methods
 NameDescription
 MethodAssertTrigger Asserts a software or hardware trigger dependent on the interface type.  
 MethodClear Performs an IEEE 488.1-style clear of the device and clears the input and output buffer (both raw and formatted I/O buffers). It also may terminate pending operations on the device.  
 MethodDisableEventDisables a client from receiving events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
 MethodDiscardEventsDiscard all pending events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
 MethodDispose (Inherited from System.IDisposable)
 MethodEnableEventEnables a client to receive events of the type specified by the eventType argument using a WaitOnEvent method. (Inherited from Ivi.Visa.IVisaSession)
 MethodLockResource Locks the resource for this session with an exclusive lock, with an infinite timeout. (Inherited from Ivi.Visa.IVisaSession)
 MethodReadStatusByte Reads the status from the device. For 488.2 instruments, this is the 488.2 status byte.  
 MethodUnlockResource Unlock the resource. (Inherited from Ivi.Visa.IVisaSession)
 MethodWaitOnEventWait for events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
Top
See Also

Reference

IMessageBasedSession Interface
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025