Keysight VISA.NET Help
IVisaSession Interface
Members 



IVisaSession is the base interface for VISA.NET I/O resources. It support capabilities for all resource types, specifically the lifetime management, locking, and identification. For more information, see Resources and Sessions.
Syntax
'Declaration
 
Public Interface IVisaSession 
'Usage
 
Dim instance As IVisaSession
public interface IVisaSession 
public interface class IVisaSession 
Requirements

Current with Keysight IO Libraries Suite 18

See Also

Reference

IVisaSession Members
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025