Keysight VISA.NET Help
IOBuffers Enumeration



Indicates buffer(s) in the low-level I/O interface. These are not the buffers used for formatted I/O. Multiple buffers may be specified.
Syntax
'Declaration
 
<FlagsAttribute()>
Public Enum IOBuffers 
   Inherits System.Enum
'Usage
 
Dim instance As IOBuffers
[Flags()]
public enum IOBuffers : System.Enum 
[Flags()]
public enum class IOBuffers : public System.Enum 
Members
MemberDescription
Read The read (input) buffer.
ReadWrite Both the read (input) and the write (output) buffers.
Write The write (output) buffer.
Inheritance Hierarchy

System.Object
   System.ValueType
      System.Enum
         Ivi.Visa.IOBuffers

Requirements

Current with Keysight IO Libraries Suite 18

See Also

Reference

Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025