Keysight VISA.NET Help
TimeoutMilliseconds Property (IVisaSession)



The I/O timeout in milliseconds for I/O communication on this resource session. If the timeout is VisaConstants.ImmediateTimeout (0), operations will never wait for the device to respond. If the timeout is VisaConstants.InfiniteTimeout (-1), I/O communication will not timeout.
Syntax
'Declaration
 
Property TimeoutMilliseconds As Integer
'Usage
 
Dim instance As IVisaSession
Dim value As Integer
 
instance.TimeoutMilliseconds = value
 
value = instance.TimeoutMilliseconds
int TimeoutMilliseconds {get; set;}
property int TimeoutMilliseconds {
   int get();
   void set (    int value);
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025