Keysight VISA.NET Help
AssertTrigger Method (IVxiBackplaneSession)



The trigger to assert.
The VXI trigger protocol to use when asserting the trigger.
Assert a software or hardware trigger.
Syntax
'Declaration
 
Sub AssertTrigger( _
   ByVal line As TriggerLine, _
   ByVal protocol As VxiTriggerProtocol _
) 
'Usage
 
Dim instance As IVxiBackplaneSession
Dim line As TriggerLine
Dim protocol As VxiTriggerProtocol
 
instance.AssertTrigger(line, protocol)
void AssertTrigger( 
   TriggerLine line,
   VxiTriggerProtocol protocol
)
void AssertTrigger( 
   TriggerLine line,
   VxiTriggerProtocol protocol
) 

Parameters

line
The trigger to assert.
protocol
The VXI trigger protocol to use when asserting the trigger.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025