| Ivi.Visa Namespace : VxiTriggerProtocol Enumeration |
'DeclarationPublic Enum VxiTriggerProtocol Inherits System.Enum
'UsageDim instance As VxiTriggerProtocol
public enum VxiTriggerProtocol : System.Enum
public enum class VxiTriggerProtocol : public System.Enum
| Member | Description |
|---|---|
| Off | Turns the associated trigger line off. |
| On | Turns the associated trigger line on. |
| Software | Sends the word serial trigger command. |
| Sync | Turns the associated trigger line on, then off. |
System.Object
System.ValueType
System.Enum
Ivi.Visa.VxiTriggerProtocol
Current with Keysight IO Libraries Suite 18