Keysight VISA.NET Help
ParseResult Class Methods


For a list of all members of this type, see ParseResult members.

Public Methods
 NameDescription
Public MethodEqualsOverloaded.  Returns True iff the given object o is a ParseResult object equivalent to this object. Two ParseResult objects are equivalent if the ExpandedUnaliasedName for the two objects have the same value with their case ignored.  
Public MethodGetHashCode Returns a suitable Hash Code for this object. The Hash Code for two objects that are Equal must be the same. The Hash Code shouldn't change over the life of the object.  
Top
See Also

Reference

ParseResult Class
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025