Keysight VISA.NET Help
Equals Method



Returns True iff the given object o is a ParseResult object equivalent to this object. Two ParseResult objects are equivalent if the ExpandedUnaliasedName for the two objects have the same value with their case ignored.
Overload List
OverloadDescription
Equals(Object) Returns True iff the given object o is a ParseResult object equivalent to this object. Two ParseResult objects are equivalent if the ExpandedUnaliasedName for the two objects have the same value with their case ignored.  
Equals(ParseResult) Returns True iff the given ParseResult object is equivalent to this object Two ParseResult objects are equivalent if the ExpandedUnaliasedName for the two objects have the same value with their case ignored.  
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025