Keysight VISA.NET Help
Equals(ParseResult) Method



Returns True iff the given ParseResult object is equivalent to this object Two ParseResult objects are equivalent if the ExpandedUnaliasedName for the two objects have the same value with their case ignored.
Syntax
'Declaration
 
Public Overloads Function Equals( _
   ByVal other As ParseResult _
) As Boolean
'Usage
 
Dim instance As ParseResult
Dim other As ParseResult
Dim value As Boolean
 
value = instance.Equals(other)
public bool Equals( 
   ParseResult other
)
public:
bool Equals( 
   ParseResult^ other
) 

Parameters

other
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025