Keysight VISA.NET Help
SerialStopBitsMode Enumeration



Specifies the number of stop bits used to indicate the end of a Serial frame.
Syntax
'Declaration
 
Public Enum SerialStopBitsMode 
   Inherits System.Enum
'Usage
 
Dim instance As SerialStopBitsMode
public enum SerialStopBitsMode : System.Enum 
public enum class SerialStopBitsMode : public System.Enum 
Members
MemberDescription
One One stop bit.
OneAndOneHalf One-and-one-half (1.5) stop bits.
Two Two stop bits.
Inheritance Hierarchy

System.Object
   System.ValueType
      System.Enum
         Ivi.Visa.SerialStopBitsMode

Requirements

Current with Keysight IO Libraries Suite 18

See Also

Reference

Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025