Keysight VISA.NET Help
VxiAccessPrivilege Enumeration



Indicates the address modifier to be used in high-level access operations when writing to the destination.
Syntax
'Declaration
 
Public Enum VxiAccessPrivilege 
   Inherits System.Enum
'Usage
 
Dim instance As VxiAccessPrivilege
public enum VxiAccessPrivilege : System.Enum 
public enum class VxiAccessPrivilege : public System.Enum 
Members
MemberDescription
BlockNonPrivileged The block non-privileged address modifier.
BlockPrivileged The block privileged address modifier.
D64DoubleEdgeVme The Double Edge VME address modifier.
D64NonPrivileged The D64 non-privileged address modifier.
D64Privileged The D64 privileged address modifier.
D64Sst160 The D64 Source Synchronous Transfer 160 address modifier.
D64Sst267 The D64 Source Synchronous Transfer 267 address modifier.
D64Sst320 The D64 Source Synchronous Transfer 320 address modifier.
DataNonPrivileged The data non-privileged address modifier.
DataPrivileged The data privileged address modifier.
ProgramNonPrivileged The program non-privileged address modifier.
ProgramPrivileged The program privileged address modifier.
Inheritance Hierarchy

System.Object
   System.ValueType
      System.Enum
         Ivi.Visa.VxiAccessPrivilege

Requirements

Current with Keysight IO Libraries Suite 18

See Also

Reference

Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025