| Ivi.Visa Namespace : VxiDeviceClass Enumeration |
'DeclarationPublic Enum VxiDeviceClass Inherits System.Enum
'UsageDim instance As VxiDeviceClass
public enum VxiDeviceClass : System.Enum
public enum class VxiDeviceClass : public System.Enum
| Member | Description |
|---|---|
| Extended | The resource belongs to the extended device class. |
| Memory | The resource belongs to the memory device class. |
| Message | The resource belongs to the message based device class. |
| Other | The resource belongs to a miscellaneous device class such as VME. |
| Register | The resource belongs to the register based device class. |
System.Object
System.ValueType
System.Enum
Ivi.Visa.VxiDeviceClass
Current with Keysight IO Libraries Suite 18