| Keysight.Visa Namespace > PxiBackplaneSession Class : ModelName Property |
'DeclarationPublic ReadOnly Property ModelName As String
'UsageDim instance As PxiBackplaneSession Dim value As String value = instance.ModelName
public string ModelName {get;}
When using multiple implementations of VISA.NET from different vendors, the value of this attribute should be used for display purposes only and not for programmatic decisions, as the value can be different between VISA implementations and/or revisions.
Current with Keysight IO Libraries Suite 18