Keysight VISA.NET Help
ReserveTrigger Method (PxiBackplaneSession)



The bus segment in which to reserve the trigger.
The trigger line to reserve.
Reserve a single trigger line that the caller can then map and/or assert.
Syntax
'Declaration
 
Public Sub ReserveTrigger( _
   ByVal bus As Short, _
   ByVal line As TriggerLine _
) 
'Usage
 
Dim instance As PxiBackplaneSession
Dim bus As Short
Dim line As TriggerLine
 
instance.ReserveTrigger(bus, line)
public void ReserveTrigger( 
   short bus,
   TriggerLine line
)
public:
void ReserveTrigger( 
   short bus,
   TriggerLine line
) 

Parameters

bus
The bus segment in which to reserve the trigger.
line
The trigger line to reserve.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025