Keysight VISA.NET Help
UnreserveTrigger Method (PxiSession)



The trigger line to unreserve.
Keysight VISA.NET does not support this method.
Syntax
'Declaration
 
Public Sub UnreserveTrigger( _
   ByVal line As TriggerLine _
) 
'Usage
 
Dim instance As PxiSession
Dim line As TriggerLine
 
instance.UnreserveTrigger(line)
public void UnreserveTrigger( 
   TriggerLine line
)
public:
void UnreserveTrigger( 
   TriggerLine line
) 

Parameters

line
The trigger line to unreserve.
Remarks
This is a standard method to unreserve a PXI trigger line, but it is not supported by Keysight VISA.NET.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025