Keysight VISA.NET Help
PxiSession Class
Members 



An instantiable class that supports all PXI INSTR sessions.
Object Model
PxiSession ClassResourceManager Class
Syntax
Remarks

PXI instrument vendors do not ordinarily expose the information needed to directly access a PXI instrument. This information is cryptic and may change from one firmware version to the next. Instead, vendors provide instrument drivers, software front panels, and other programs for instrument access. Under normal circumstances, instrument users should not attempt to access PXI instruments using this class.

Inheritance Hierarchy

System.Object
   Keysight.Visa.VisaSession
      Keysight.Visa.RegisterBasedSession
         Keysight.Visa.PxiSession

Requirements

Current with Keysight IO Libraries Suite 18

See Also

Reference

PxiSession Members
Keysight.Visa Namespace

 

 


© Keysight Technologies 2015-2025