Keysight VISA.NET Help
ResourceManager Class Properties


For a list of all members of this type, see ResourceManager members.

Public Properties
 NameDescription
Public PropertyFindExportedResourcesOnlyDetermines whether only those sessions with property VisaSession.ExportEnabled = true will be returned from the Find and Parse methods. (Keysight Specific)  
Public PropertyImplementationVersion The version of this VISA.NET implementation.  
Public PropertyIOLibrariesPath The full pathname of the Keysight IO Libraries directory used by this implementation of Keysight VISA.NET. The pathname returned varies, depending on whether the process is a 32-bit or 64-bit process. (Keysight Specific)  
Public PropertyIOLibrariesRegistryKey The full pathname of the Keysight IO Libraries registry key used by this implementation of Keysight VISA.NET. The pathname returned varies, depending on whether the process is a 32-bit or 64-bit process. (Keysight Specific)  
Public PropertyManufacturerId The Keysight VISA.NET manufacturer ID - '4095'.  
Public PropertyManufacturerName The VISA.NET vendor name - 'Keysight Technologies, Inc.'.  
Public PropertyReturnAllDetermines whether Find will return all discovered instruments or just those that are in My Instruments list. The default value is false, meaning Find will return only My Instruments. Use Connection Expert to add My Instruments; by default, all locally-connected (non-LAN) instruments and all manually-added instruments are in My Instrument list. (Keysight Specific)  
Public PropertySpecificationVersion The version of the VISA.NET specification with which this VISA.NET implementation complies.  
Public PropertyVisaFrameworkPath The full pathname of the VISA Framework directory used by this implementation of Keysight VISA.NET. The pathname returned varies, depending on whether the process is a 32-bit or 64-bit process. (Keysight Specific)  
Top
See Also

Reference

ResourceManager Class
Keysight.Visa Namespace

 

 


© Keysight Technologies 2015-2025