Keysight VISA.NET Help
Open(String) Method



The VISA resource name.
Creates a VISA I/O resource session.
Syntax
'Declaration
 
Public Overloads Function Open( _
   ByVal resourceName As String _
) As IVisaSession
'Usage
 
Dim instance As ResourceManager
Dim resourceName As String
Dim value As IVisaSession
 
value = instance.Open(resourceName)

Parameters

resourceName
The VISA resource name.

Return Value

A reference to VISA.NET session for the specified resource.
Remarks

Some Keysight IO Libraries Connection Expert settings and Keysight Instrument Discovery Service policies affect the operation of Open. Refer to the IO Libraries Suite Help for more details.

For instruments that are auto-discovered by the Discovery Service, Open verifies that the instrument is present.

For instruments that are manually-added, Open does not verify the presence of the instrument. If the device is not present or not turned on, you will not discover this until you attempt to communicate with the instrument.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025