Keysight VISA.NET Help
Parity Property (SerialSession)



The parity used with every frame transmitted and received.
Syntax
'Declaration
 
Public Property Parity As SerialParity
'Usage
 
Dim instance As SerialSession
Dim value As SerialParity
 
instance.Parity = value
 
value = instance.Parity
public SerialParity Parity {get; set;}
public:
property SerialParity Parity {
   SerialParity get();
   void set (    SerialParity value);
}
Remarks

The default is Ivi.Visa.SerialParity.None.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025