| | Name | Description |
 | BaudRate |
The baud rate of the interface.
|
 | BytesAvailable |
The number of bytes available in the global receive buffer.
|
 | ClearToSendState |
The current state of the Clear To Send (CTS) input signal.
|
 | DataBits |
The number of data bits contained in each frame (5, 6, 7, or 8).
|
 | DataCarrierDetectState |
The current state of the Data Carrier Detect (DCD) input signal.
|
 | DataSetReadyState |
The current state of the Data Set Ready (DSR) input signal.
|
 | DataTerminalReadyState |
The state of the Data Terminal Ready (DTR) output signal.
|
 | EventQueueCapacity |
The maximum number of events that can be queued at any time on this session. The default
is 50.
(Inherited from Keysight.Visa.VisaSession) |
 | ExportEnabled | Together with the Keysight ResourceManager.FindExportedResourcesOnly property, determines whether the resource associated with this session instance is reported by the Keysight Find and Parse methods. (Inherited from Keysight.Visa.VisaSession) |
 | FlowControl |
The flow control mechanism(s) used by this serial connection.
|
 | FormattedIO |
A reference to the Formatted I/O interface. Keysight VISA.NET uses the standard Formatted
I/O implementation provided by the IVI Foundation in the VISA.NET Shared Components.
(Inherited from Keysight.Visa.MessageBasedSession) |
 | HardwareInterfaceName |
A human-readable description of the hardware interface associated with this session.
(Inherited from Keysight.Visa.VisaSession) |
 | HardwareInterfaceNumber |
The board number of the hardware interface associated with this session.
(Inherited from Keysight.Visa.VisaSession) |
 | HardwareInterfaceType |
The type (GPIB, ASRL, etc.) of the hardware interface associated with this session.
(Inherited from Keysight.Visa.VisaSession) |
 | InternalHandle |
The VISA C handle to the underlying VISA C session.
(Inherited from Keysight.Visa.VisaSession) |
 | IOProtocol |
The protocol type for I/O communication with the device. This property applies to this
session only (VISA local scope).
(Inherited from Keysight.Visa.MessageBasedSession) |
 | Parity |
The parity used with every frame transmitted and received.
|
 | RawIO |
A reference to the raw (no formatting) I/O interface.
(Inherited from Keysight.Visa.MessageBasedSession) |
 | ReadTermination |
The method used to terminate read operations.
|
 | ReplacementCharacter |
The character used to replace incoming characters that arrive with errors (such as
parity errors).
|
 | RequestToSendState |
The current state of the Request To Send (RTS) output signal.
|
 | ResourceClass |
The resource class of the currently open resource. Possible values are INSTR, INTFC, MEMMAC,
SOCKET, and BACKPLANE.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceImplementationVersion |
The version of this Keysight VISA.NET implementation.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceLockState |
The state of the resource-wide lock on the currently open resource.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceManager | A private instance of the ResourceManager created when this session was instantiated, and available until this session is disposed. (Inherited from Keysight.Visa.VisaSession) |
 | ResourceManufacturerId |
The VXI manufacturer ID of the software vendor of this VISA.NET implementation - '4095'.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceManufacturerName |
The name of the software vendor that corresponds to the ResourceManufacturerId property -
'Keysight Technologies, Inc.'.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceName |
The VISA resource name of the currently open resource. This name is the canonical version
of the resource name and therefore may vary from the resourceName parameter used to
instantiate the session.
(Inherited from Keysight.Visa.VisaSession) |
 | ResourceSpecificationVersion |
The version of the VISA.NET specification that describes the functionality provided by this
session class.
(Inherited from Keysight.Visa.VisaSession) |
 | RingIndicatorState |
The current state of the Ring Indicator (RI) input signal.
|
 | SendEndEnabled |
Enables/disables sending the END signal on the last byte of a write. This property applies
to this session only (VISA local scope).
(Inherited from Keysight.Visa.MessageBasedSession) |
 | SessionType |
The type of the current session.
(Inherited from Keysight.Visa.VisaSession) |
 | StopBits |
The number of stop bits used to indicate the end of a frame.
|
 | SynchronizeCallbacks |
Specifies whether callbacks must be performed in a specific synchronization context. If false,
the implementation is allowed to execute callbacks in any context. The default value is true.
This property applies to this session only (local scope).
(Inherited from Keysight.Visa.VisaSession) |
 | TerminationCharacter | The ASCII character used to end reading. This property applies to this session only (VISA local scope). (Inherited from Keysight.Visa.MessageBasedSession) |
 | TerminationCharacterEnabled | If true, read operations end when a termination character is received. This property applies to this session only (VISA local scope). (Inherited from Keysight.Visa.MessageBasedSession) |
 | TimeoutMilliseconds |
The I/O timeout in milliseconds for I/O communication on this resource session.
(Inherited from Keysight.Visa.VisaSession) |
 | WaitForLockRelease |
Indicates whether methods and properties from this session instance will wait for a timeout
period for a resource lock to be released (true) or not (false).
(Inherited from Keysight.Visa.VisaSession) |
 | WriteTermination |
The method used to terminate write operations.
|
 | XOffCharacter |
The value of the XOFF character used for XON/XOFF flow control (both directions).
|
 | XOnCharacter |
The value of the XON character used for XON/XOFF flow control (both directions).
|