Keysight VISA.NET Help
WriteTermination Property (SerialSession)



The method used to terminate write operations.
Syntax
'Declaration
 
Public Property WriteTermination As SerialTerminationMethod
'Usage
 
Dim instance As SerialSession
Dim value As SerialTerminationMethod
 
instance.WriteTermination = value
 
value = instance.WriteTermination
public SerialTerminationMethod WriteTermination {get; set;}
public:
property SerialTerminationMethod WriteTermination {
   SerialTerminationMethod get();
   void set (    SerialTerminationMethod value);
}
Remarks

The default is Ivi.Visa.SerialTerminationMethod.None.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025